Part Number: TPS65988
Other Parts Discussed in Thread: TPS65987, TPS65987D
Hi,
We use TPS65988DH chip with port 2 setup as DisplayPort Sink, GPIO4 is used as HPD input.
Our DP sink generates HPD pulse with different width and sends it to GPIO4 HPD input. If pulse width is more than 4 ms, tps65988 transmits USB-PD message with Alt DP Attention command. But after sending a HPD with pulse width 2.2 ms, tps65988 will not transmit any USB-PD message with Alt DP Attention command any more.
To restore functionality need to power cycle or issue GAID command.
The problem looks very similar to
e2e.ti.com/.../tps65988-dp-alt-mode-sink-gets-stuck-after-sending-4-and-4-8-millisecond-hpd-pulse
Has this problem been solved already?