Part Number: AM26C31
Other Parts Discussed in Thread: AM26LS31
Hello Guys,
Good day.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM26C31
Other Parts Discussed in Thread: AM26LS31
Hello Guys,
Good day.
Our customer is using AM26C31 in their encoder, but when they test the current between channel pairs (they use 120 ohms between the channel pairs), the current measured is around 23-24 mA. However, based on the datasheet, the current should be limited within 20mA only.
What could be the reason? They are asking because their customer asked for current limitation with 20mA.
Note that the channel pairs measurement were done between pin2 and pin 3, between pin 5 and pin 6, between pin 10 and pin 11 and as such.
Thanks and regards,
Art
Thanks Hao!
Art,
AM26LS31 has the similar driving strength as AM26C31. The Voh/Vol spec ((2.5V-0.5V)/20mA) is equivalent to 2V Vod over 100Ohm (RS-422 standard).
With heavier load (for example 54Ohm), the devices may not meet the min 1.5V standard of RS-485. But as long as the receiver side has enough margin over its threshold, the communication should work fine.