Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987,
Hi Team,
Our customer is using TPS65987 for negotiating highest power available from external USB-C charger power source (no USB data, no alternate mode). Before any connection, TPS65987 is in dead battery mode (no VIN_3V3). Can you help with the questions below, thanks in advance.
We are having difficulty detecting whether the device was woken up by a charger attach event. When booting from "dead battery" with the charger connected, after the patch file is loaded I read the Power Status Register (0x3F) and it is all 0's ( PowerConnection = No Connection, Charger Detect Status = Charger detection disabled or not run, etc). This has our firmware believe that we booted without a cable attached which puts us in an undesired state. Is there a reliable way at startup to detect that the charger is connected without an arbitrary wait time?
Thanks and regards,
Don