Hi expert,
I'd like to ask for your help to understand the PU/PD configuration. As per the related thread :
Device has internal PU/PD of 9k , hence can be left floating. However if you want to be have extra safety on design, you can always have external PU/PD. Hope this is clear. You can use PU/PD thru 2.2K resistor.
1. Could you kindly give me more information why external 2.2k of PU/PD resistor adds extra safety on design? I wonder why the device requires the external PU/PD resistor even though the device itself already internally support it.
2. Additionally, I'm going to use 10kohm PU resistor on INT/PWDN pin and RESET_N pin instead of 2.2k which is recommended in DS. Could you advise the possible effect here?
Thank you for your help!