Part Number: DP83867CR
Hi Adrian,
We made a setup of our board with 20 ohm series resistors on the RX lines and with the reset signal disconnected completely from the processor (cut the trace and left it just with the external pullup). This way the device seemed to be working ok with stable connection always.
We sent the board to our client in order to modify Firmware to handle Reset Signal. So they reconnected reset and after they made firmware modifications they reported that “the device was sometimes working and sometimes bad values (Device-ID) is answered from phy”.
Do you have any idea why this could happen? Does it seem to you like a hardware issue or a possible bad handling from the firmware side?
Regards,
Ioannis