This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: Power pin connections

Part Number: TPS25750
Other Parts Discussed in Thread: USB-PD-CHG-EVM-01

Dear TI team,

I am planning on using the TPS25750D in a sink-only configuration with dead battery mode (the device does not have a battery and is powered purely through USB Type-C). I wanted to double-check that it is OK to leave the PP5V, VBUS, and VIN_3V3 pins unconnected in this case, correct? Furthermore, there is no need to add decoupling capacitors on these pins in this case, is there?

Kind regards,
Marcis