Part Number: SN65DSI86
Other Parts Discussed in Thread: TEST2
Hi ,
I am planning to use eDP 1.2 version LCD display (2 lanes of eDP ) with SN65DSI86 (with only 4 lanes of MIPI DSI input) . Let me know:
1. Is SN65DSI86 can support eDP1.2 version display (2 lanes for data, without Panel self refresh PSR and without ASSR) ?
2. The resolution of the display is 1920 x 1200 @ 60 , color is 8 bit (24bpp) .The maximum pixel clock frequency = 158.73MHz. (2160x 1212x60 ) . Is it possible to stream total LCD data through 2 lanes of eDP interface.
Regards
PSG_4