Other Parts Discussed in Thread: XIO2001
Hello,
we use the XIO2001 to build a PCIe card and connect the bridge to a PCI core. Using DMA we copy data from the card to the RAM of the PC. About 5 minutes after starting the operation, the PC freezes. No dump file is created. Our PCI traffic looks normal until that point.
System:
Windows 7 Embedded Standard 64 Bit
Intel Core i7 610 (Arrandale)
Chipset Ibex Peak (QM57), supports PCIe 2.0
We found 2 workarounds:
-Disabling PCIe ASPM completely in the energy options.
-Disabling PCIe ASPM for the XIO2001 in Windows registry
We tried several combinations of PCIe ASPM L0s/L1 activation and L0s/L1 latencies, but no effect. (According to PCIe 2.0 spec, L0s may not be disabled.)
I saw the earlier post in the forum, "Does the XIO2000A work in PCIe 2.0 slots?"
It is mentioned there that a chipset driver update might fix some PCIe issue, but it didn't work for me.
Disabling ASPM is not a clean option.