This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
Please allow me to ask you about the pull-up and pull-down resistor value for TMDS181 control pins. I see below table in the datasheet.
It says, "Control pin MIN/MAX voltage for High/Low".
[Q1] Does this mean that the pull up or pull down resistor value must be smaller than 65k ohm ?
[Q2] What happens when user uses 68k ohm ?
[Q3] What happens when user uses 10k ohm ?
Best Regards,
Kawai
Hi Kawai-san,
Control pins were designed using 65k pull-up/pull-down values around it will work fine, 68k is close enough.
10k is too low; it may cause the device to lose its configuration.
Regards
Hello Moises-san,
Please allow me to double check for each cases.
Pull-Up
Q1). What is the required accuracy for the 68k pull up resistor ? I believe it must be in certain range of 65k ohm.
Pull-Down
Q2) What is the required accuracy for the 68k pull down resistor ?
Q3). I believe pull down could be a smaller resistance. Is 10k or 1k pull down acceptable ?
Best Regards,
Kawai