Other Parts Discussed in Thread: DP83640
Hello,
I am trying to run a project requiring PTP protocol. I have two DP83640-EVK and connect with CAT-5 cable.
I tried to use ALP to do Phase Alignment (from AN-1729 3.2 Phase Alignment). Two boards are connected with USB ports to the same laptop.
There is a post which tried something similarly. It seems the post did not succeed in repeating what the tutorial does.

First of all, I want to clarify is the current setup ( two DP83640-EVK connecting with CAT-5 cable) enough to repeat the phase alignment experiments?
Second, I did not use Enable Synchronous Ethernet mode, because my understanding is that it can improve the resolution, but it is ok to sync the signal without it.
I basically repeated the tutorial and like the post I mentioned, there is nothing happened.
There might be something I missed? Because in the document, there is no clear instruction to set the master and slave between two boards. Therefore, I am not even sure, two boards are communicating. Furthermore, by watching this demo video,
I feel like to phase alignment is not as simple as what tutorial describes, because the hardware setup is not mentioned at all.