Other Parts Discussed in Thread: DP83640
Hi,
I have DP83640 PHY on board connected to MAC via RMII. LED link is lit and ACT is blinking, but pinging gateway doesn't work. Any idea what may be wrong?
Kind regards,
Jacek
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ross,
Thanks for your email, I've sent you schematic files and register settings.
Getting a bit more into details we are trying to make DP83640 working with SFP modules. You have two versions of schematic, one is for copper ethernet (proper copper with transformer, RJ45 and so on), second one is for SFP module. Also you have two sets of register settings, one is for copper and one for SFP. Board with SFP modules is working fine, but it doesn't work with copper ethernet. Can you advise what's wrong, please?
Regards,
Jacek.
Hi Ross,
0x01 - 0x78E9, 0x78ED
0x10 - 0x6E15.
When cable is connected I can see LINK LED lit and ACT LED blinking. Maybe it will attract your attention that I'm getting big number of errors while pinging:
eth0 Link encap:Ethernet HWaddr 02:D0:93:2B:91:F0
inet addr:192.168.10.229 Bcast:192.168.10.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:77 errors:72 dropped:10 overruns:0 frame:72
TX packets:51 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:8832 (8.6 KiB) TX bytes:0 (0.0 B)
Regards,
Jacek.
Hi Jacek
Thank you for your answer. I'm designing in Altium with DP83640 EVB schematic for a FIBER. Could you take a look at my schematic with DP83640? Jacek is a polish name so I thought that you are in Poland - like me.
Best regards
Paweł
Hi Jacek
I bought DP83640T Evaluation Demo Board and I connect it to an Evaluation board with microcontroller. With copper every think is all right. But SFP doesn't work. I changed resistors on board for a fiber, I put RXER to the ground with 2.2 resistor. I have no idea what is going on. Do I need to change something in PHYs registers for a SPF?
Best Regards
I assumed that you have fiber at DP83640 end, then it goes through media converter and the other end is copper. So on copper end (i. e. computer) autonegotioation (10/100) has tu be turned off, that is it has to be set to either 10 or 100 according to what is fiber end set. This is because that two stations can't autonegotioate speed.