Part Number: TUSB9261
Other Parts Discussed in Thread: TUSB8020B, , HD3SS3212
Help would be much appreciated.
I have integrated the TUSB9261 and TUSB8020B into a custom circuit. At the moment, everything functions correctly without an SSD connected. I can plug into Windows 10 and flash the firmware with ease. I've switched the TX polarities just like in the reference design, and have tried all the different firmware flavors (RX, TX, None, Both) just in case there is a mixup.
The SSD I'm using is the Samsung EVO 850 (256GB). Powering that over 5V and trying to make some headway here. Whenever I plug it in, a few new lights try to flash (starting USB 3.0, etc) and then the module seems to reset. This isn't working.
Can someone provide some helpful reasons of things I might need to check?