Part Number: DP83822I
We are using DP83822 (single port 10/100 Mbps Ethernet PHY Transceiver) connected to PowerPC Processor MPC8360 in one of our designs. The electrical interface (RJ-45) is tested and is working fine. We have made necessary Hardware modifications to connect to the Fiber Interface. But we are facing issues while configuring the Fiber interface (100 Base-FX, Full-duplex). We are connecting it to a 1Gbps Ethernet tester through SFP. The ping is not working. Attached Schematic pages (Electrical interface & Fiber interface separately after modifications).