Part Number: DS80PCI402
Hi Sir,
I want to design DSP80PCI402 as a master in I2C mode and connect with an EEPROM.
I have several questions in mind.
1. Is the AT24C04C EEPROM from Microchips compatible in this application?
2. is that okay if i program EEPROM with both EEPROM and DSP80PCI402 power on. note that the SCL and SDA for both devices are connected.
3. If question 2 is feasible, what precaution should i take to prevent miscommunication and damage to the DSP80PCI402.
Thanks you.
-Desmond