Hi,
For the 16 pin layout of ISO1042-Q, there are several not connected pins.
Is it possible to use NC pins connected to ground (low or high)? What are the consequences?
Thanks in Advance
Emre
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For the 16 pin layout of ISO1042-Q, there are several not connected pins.
Is it possible to use NC pins connected to ground (low or high)? What are the consequences?
Thanks in Advance
Emre
Hi Emre,
Welcome to TI E2E Forum!
Thank you for reaching out and for your interest in ISO1042-Q1. The NC pins are not connected to the die internally, hence, they can be connected to VCC, GND or left open without any issues. Hence, please go ahead and connect them with any of the three options, according to your convenience. Thanks.
Regards,
Koteshwar Rao