This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW7742: ISOW774x do support signal level translate?

Part Number: ISOW7742

Dear Sir/Madam,

I would like to confirm that ISOW774x does support isolated signal-level translation?

e.g. Digital side with 1.8V I/Os. Isolated side with 3.3V I/Os, with VIO pin = 1.8V, Vdd pin = 3.3V, VSEL pin = GND2, VISOOUT pin = 3.3V output & feed to VISOIN pin.

From the Electrical Characteristics 7.11~7.18, all those characteristic cases are the same supply voltage between VIO & VISOIN. Not sure do accept different supply voltage between VIO & VISOIN.

Thanks for your time on this support.

Best regards,

Ping