Dear team,
what is the recommended input capacitance on input of DCDC portion of the ISOW family?
Thanks and best regards,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
what is the recommended input capacitance on input of DCDC portion of the ISOW family?
Thanks and best regards,
Michael
Hi Michael,
Thanks for reaching out.
The minimum decoupling capacitor combination that we recommend on VDD pin of ISOW7744 is "10µF + 0.01µF", as also stated in the datasheet under section "Layout Guidelines". We also suggest that an additional 1µF is also used to support better filtering and maintain a stable supply. You can also refer to the below application note for more details on the schematic and PCB layout guidelines, thanks.
How to Meet CISPR 32 Radiated Emissions Limits With ISOW7741 |
Regards,
Koteshwar Rao
Hi Koteshwar,
thanks for your quick response and sending the app note.
Best regards,
Michael