This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
1. Capacitor value
On EVM, a Murata cap is applied as C4. Do we have some recommendation on DC bias and initial tolerances? Also is there a lower limit?
*C4: GRM21BR6YA106KE43L (+/-10% Initial Tolerance, -37.3% DC Bias (@5V))
10uF x (-10%) x (-37.3%) = 5.6uF
2. 13.1 Layout Guidelines
It says no traces or grounding within 4 mm, is this origin recognized from copper to 11pin, 12pin?
If a 4 mm circle is added to the EVM layout, why would there be a pattern inside the circle around L5?
3. 13.2 Layout Example
What is the reason for the 2-4mm limitation between capacitors?
If the passcon is moved away from the power supply pin, it may affect the stability of the power supply. What happens if the passcon is moved closer to the power supply pin?
Best regards,
Shotaro
Hi Shotaro-san,
Thank you for reaching out.
You probably missed to attach the schematic, so I am not sure which ones are C4 and L5 but I will still be able to answer your questions. Please find my inputs below,
Regards,
Koteshwar Rao
Hi Rao-san,
Thank you for supporting.
I think that the DC bias information comes from the below URL.
https://www.murata.com/en-global/products/productdetail?partno=GRM21BR6YA106KE43%23
Best regards,
Shotaro
Hi Shotaro-san,
Thank you for sharing the link, this helps.
This behavior is similar for most capacitors and hence, this is okay. Thanks.
Regards,
Koteshwar Rao