I want to confirm if it is ok that I design for output higher than 30V, like 31V?
If not ok , what limits the output, the internal MOSFET?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to confirm if it is ok that I design for output higher than 30V, like 31V?
If not ok , what limits the output, the internal MOSFET?
Hello Xiang,
Thank you for reaching out. The SN6505B-Q1 can be designed for 31V. Your transformer selection will dictate what voltage is on the secondary side. However please note that power has to be conserved, so if the input is 5V @ 1A the output at 31V will be ~160mA (transformer losses not included).
As you have noticed the topology in figure 9-11 can be used to help make the most out of your turns ration and quadruple Vin. However, the output will still be limited by power, so the total system will not exceed 5W.
Best,
Andrew