This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
We are using CAN Transceiver IC in our design. The purpose of this ISO1042BDWVR CAN Transceiver as a loopback CAN and UART Test.
Kindly find below image for your reference.
Power Supply :
Kindly let me know if any change require power side.
Thank & Regards,
Vishal
Hello Vishal,
Thanks for reaching out. The ISO1042BDWVR can support a VCC1 at 1.8V. However, the data sheet reccomended operating conditions for VCC2 is 5V only (the 4.5V - 5.5V range). Based on the schematic, it also looks like the MCP2562FD is also using a VDD of 5V for the CAN bus and a VIO of 3.3V for the logic inputs.
Let me know if you have further questions.
Best,
Andrew