This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7741-Q1: SPICE model of ISO7741FQ required.

Part Number: ISO7741-Q1
Other Parts Discussed in Thread: ISO7741,

Hello TI team,

Could you please help me with the PSICE model of ISO7741FQ, the product webpage contains only the model of ISO7741.

The F-suffix component has default output state "LOW" and the other has default state as "HIGH"

Image taken form datasheet of ISO7741FQDWRQ1.

  • Hello,

    Thank you for your inquiry.

    Th PSPICE model is located in the ISO7741-Q1 product page under the Design and Development ---> Design tools & simulation tab: ISO7741-Q1 data sheet, product information and support | TI.com.

    This PSPICE model is applicable to both the F suffix (ISO7741-Q1) and non-F suffix (ISO7741F-Q1) devices. 

    I see you had some trouble referencing the ISO7741F for the E2E post. In order to add a part number to the E2E post, please use the entire part number or the part number you see on the device's product page.

    Regards,
    Aaditya Vittal