This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6507: SS/ILIM voltage level after soft start

Part Number: SN6507

hi

I need to select the voltage rating of the Css capacitor.

What is the maximum voltage at the SS/ILIM pin?

I suppose it depend of Rlim.

In my application, Rlim is 18.2kOhm.

During soft start, Iss is 275uA. What is this bias current afer soft start?

BR