Other Parts Discussed in Thread: ISOM8110, ISO6721
Hi,
We are developing a Energy Monitoring device. Energy Monitoring IC communication pins are directly connected to CC3220MODSF12MOBR (MCU). Neutral will be connected to MCU GND and common VDD used for MCU and Energy Meter IC.
4 to 20mA output and 0-10VDC Output Sensors will be connected to MCU. We are having Following Query;
1. Neutral will not be affect the performance, Working of the MCU in the RF,EMI prospective for the Wi-Fi communication, right?
2. We need to provide the Isolation between Sensors and AC signal (Neutral) for safety prospective. So we are thinking to Provide the Isolation between the Sensor Port and MCU. We aware we can use Isolators in Digital signal like SPI,I2C,etc, but we are not sure we can use Isolators in Analog signals. So kindly advice, Can we use the Isolators between Sensor output and ADC pin of the MCU? Any degradation of Analog signal? If we can use the Isolators, kindly suggest the Isolator IC.
Thanks and regards,
Naveen K