Part Number: ISO1640
Tool/software:
Hello,
I'm working with bidirectional communication (0-3.3 V), so communication over one wire can go in both ways. I have to isolate 4 channels, so four wires with bidirectional communication. Is there any isolator for 4 channels that you can suggest it? Usually there are isolators for one way communications.
Would be ISO1640 an appropriate one? I know that I need to use two of them to isolate 4 channels, but the problem I see with this isolator is offset on the Side 1. It would be great to don't have it, but I understand that this isolator was developed to isolate I2C communication lines.
Many thanks,
Kind regards,
Dejan.