Part Number: ISOW7742
Other Parts Discussed in Thread: ISO1432, ISO7842, ISOW7741, SN6501,
Tool/software:
Hello Folks,
We need to select a single-ended isolator, and note that TI is offering two different solutions.
the 78xx series seems to have the Viso connected internally, and requires only decoupling.
the 77xx series seems similar to the ISOW14x2 series with the isolated supply fed back to the device externally.
From an EMC, power consumption, or other factor, can one be recommended over the other? If they are the same, we prefer the smaller package as our board is dense.
Edit:
Another semi-related question: For the 78xx series, it seems there is an excess of Viso capacity when operating from 5V. Very curious if we could power 1 or 2 ISO1432 from this supply to limit dissipation to one component for the Viso supply. This all is related to helping us a: protect that GPS module mentioned in our other question, and b: helping to create a more compact layout given the challenging real estate!
Very curious if this is not advisable for some reason.
Much thanks for the wisdom!