Part Number: ISO3086
If the pi1,2 is NC, the ISO3086 chipset can do normal operation?
VCC1, VCC2 is connected to each 3.3v and 5V, They are isolated DC powers.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.