Other Parts Discussed in Thread: ISO7710, ISO7041, ISO7021, SN74LVC2G17-Q1, ISO7731-Q1, ISO7742-Q1, SN74LVC1T45-Q1, CD40109B-Q1, ISO7742, CD40109B, ISO122, ISO224
Hi TI Team,
I wanted to Isolate ADC input pins which is coming from external circuitry, Its a single pin ADC, where its voltage will be 0 to 12V max. but my SOC accepts only 1.8V levels of ADC data
So I need Isolation, voltage translation and then buffer.
Note(not looking for differential ADC input Isolators)
So please suggest me the parts for the above requirements.
Manjunath