This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1410: Is ISO1410 pin to pin with ISO3082

Part Number: ISO1410
Other Parts Discussed in Thread: ISO3082,

Hi, 

Compared ISO1410 and ISO3082, I found pin11~14 is not the same, can these two device pin to pin replace? Thanks.

Best Regards,

Chen

  • Hi Chen,

    Thank you for posting to E2E! Since the ISO1410 is a half-duplex device, it is pin-to-pin compatible with ISO3082 as shown in the images below:

    ISO3082 pinout:


    ISO1410 pinout:



    Respectfully,
    Manuel Chavez