Other Parts Discussed in Thread: UCC5304, ISO7762, , AMC1336
hi, I need to know if the below devices are in LOW voltage mode at the start.
UCC5304
ISO7762
ISO7742-Q1
thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi, I need to know if the below devices are in LOW voltage mode at the start.
UCC5304
ISO7762
ISO7742-Q1
thank you!
Hi Daniel,
There isn't anything like low voltage or high voltage mode for the isolators. The isolators have isolation barrier built-in permanently and support the full isolation voltage at all times whether powered or unpowered.
Let me know if it answers your question, thanks.
Regards,
Koteshwar Rao
thank you.
i have also a question regarding AMC1336.
i want to use it to sample wide input and i am sure that i will have a noise in the input. - can i work with a buffer before the positive input?
and also can you let me know what will be the error according to the noise? it is possible to get 1 Volt error because of the noise?