Other Parts Discussed in Thread: ISO1540
Hi,
I am having trouble understanding the difference between VIH1 and VIHT1.
As can be seen from the recommended operation conditions (Table 6.3), for VCC1 = 3.3V,
2.31V < VIH1 < 3.3V
From electrical characteristics (Table 6.9),
0.54V < VIHT1 < 0.7V
Same doubt goes for the other voltage levels too, namely VIL1- VILT1, VIL2 - VILT2, VIH2 - VIHT2.
Which of these tables should I consider for checking my logic level compatibilies while interfacing with I2C or SMBus devices