This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you advise if below signal from RS485 A/B pins ( 12 and13 ) using ISO3082 is normal. Said ISO3082 part is already communicating with my slave device but I just noticed that the waveform does not have thesame amplitude.
Is this normal and is there any concern on this one? If this is a concern, any idea how to fix this?
Thanks,
Norman
Hi Norman:
Thanks for posting your question on E2E.
Unfortunately, your waveforms didn't get attached to your post. Could you please add the image to this thread again? You may follow these steps when attaching an image.
In addition, please be sure to include following information.
Lastly, you may consider our latest ISO1410 (P2P with ISO3082) and/or ISO1500 (smaller package option) for your newer designs.
Regards,
Dushmantha
Hi Dushmantha,
Please see below:
Hi Norman:
Thanks for reattaching the waveforms and providing the additional details.
Yes, this (A-B) output amplitude is lower than expected. I'd expect the amplitude to be about +/-2.3V with 60Ohm effective termination and under nominal conditions (Vcc2=5V and room temperature).
In order to debug this, can you please share the A and B output single ended waveforms (probed with respect to GND2)?
Can you also share the following information?
Thanks,
Dushmantha
Hi Dushmantha,
I did some more verifications on my side and found out the Vcc2 should be 5V and I was using only 3.3V. It did improve the signal levels but it is not exactly thesame amplitude. I tried to play around with R27 ( IS03082 A/B ) termination and found that 470R makes the level more equal but in this case the termination is now imbalance. I did check/compare the amplitude at both A/B end pins of both ISO3082 and MAX3079EESD+T devices at thesame time and they are exactly thesame. Not sure what can be the concern if i leave 120R/470R termination with equal amplitude on both A/B ends against 120R/120R termination with 200mV amplitude difference. In my application, I only use one slave device nothing in parallel.
Note: there is an error on R26 and R28 connections but in this case I just remove them for the mean time including making R19/R20 change from 10R to 0R.
Hi Norman:
It's great to hear that the A-B signal amplitude is within expectations after changing the Vcc2 supply to 5V. Please note our ISO3082 Vcc2 should be between 4.5V and 5.5V for the correct operation.
200mV delta between the two transceivers are expected due to the device differences. You don't have to match the primary and secondary side amplitudes tor the correct operation of your system. RS-485 is a robust physical layer. All RS-485 transmitters will output >1.5V output swing with 60-Ohm termination. Receiver inputs can recognize signals as low as 200mV over a common mode range of -7V to +12V.
I'd recommend that you keep 120R/120R termination for the best signal integrity.
Regards,
Dushmantha