Other Parts Discussed in Thread: SN6501
Hi team,
My customer met question as following when they used SN6505B,could you please help it? Thanks!
Question 1: In Figure 1, is the requirement of voltage * time value corresponding to the unipolar application parameter or bipolar application parameter (see the red line part of the recommended WE transformer parameter in Figure 2)?
Question 2: How many parameters are there between the unipolar application parameters and bipolar application parameters of the red line part of the WE transformer parameter? (Eg unipolar application parameter is voltage between PIN 1-2 * time parameter; bipolar application parameter is voltage between PIN 1-3 * time parameter)
Question 3: Please help confirm whether the CGDT75 transformer in the attachment is used in SN6505B application, can it meet the application of 100mA current?