Hello,
Could you please let me know the minnimum regulation current of TPS92630-Q1 / TL4242-Q1 ?
I understood that this device outoput current(min) is 10mA/ch.
However our customer request the 3mA(min) +/- 5% for tail lamp.
If these devices can't use with 3mA , could you please let me know other device? (TPS92638-Q1 achieve the requirement?)
Or, can we achive the requirement by additional circuit?
Specifications are the following.
Vin:10V ~ 16V
ILED: 3~10mA for tail 120mA for stop.
Vf:1.8V~3V
LED#: 3Series, 3Parallel
Best Regards,
Ryuji Asaka