Hi, all.
The ripple voltage at light load by low temperature of TPS61240-Q1 is too big.
Our condition and result are below
Vin=3.3V, Vout=5V
Iload=0.5mA
Ta=25C Vripple=20~30mV
Ta=-40C Vripple=240~250mV
Please see the attached file too.TPS61240-Q1.pptx
Please tell me the following two specification.
1. Temperature dependency of the target voltage in the PFM mode.
2. Temperarure dependency of the ripple voltage in the PFM mode.
Best Regards,