We have a technical-type question about the output capacitance of the LM158AHRLQMLV amplifier. What is the output capacitance of the amplifier between pin 4 and 7? Our customer has a hard limit of 100pF, we have some capacitance in parallel (18nF), and we need to know about how much is going to be contributed by the amplifier. Any guidance regarding this value would be most appreciated.
Our amplifier output voltage will vary between -1 and 7 VDC.