This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TLC77-EP: TLC7701MPWREPG4 ELECTRICAL CHARACTERISTICS Information.

Genius 3530 points

Replies: 3

Views: 664

Hello

I'm Not Found the Negative-going input threshold voltage and Min Value of Delay time for TA = -55°C to 125°C(TLC7701) at datasheet.

Please Can you tell me the this ELECTRICAL CHARACTERISTICS?

and Is V62/04604-04XE rating the Military Grade?

Regards.

  • Hello Louis,

    I will look into seeing if we have the data for the higher temperature ranges for the TLC7701 and TLC7705. Were you looking for one of the devices in particular?

    As far as the military rating, the VID does not indicate military grade but is used to help track an enhanced device. You can find the VID (Vendor item drawing) datasheet at landandmaritimeapps.dla.mil/.../V6204604.pdf. You can find more information about VIDs at e2e.ti.com/.../5238.What-is-a-Vendor-Item-Drawing.pdf.

    Thanks,
    Kyle

  • In reply to Kyle Rakos:

    Hello Louis,

    The minimum and maximum are the same for the TLC7701 for both the -40C to 125C part and -55C to 125C parts. The data for the TLC7733 is listed on the ti.com datasheet.

    Thanks,
    Kyle
  • In reply to Kyle Rakos:

    Hi Kyle

    Thank you for your support.

    Regards.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.