Hello,
I would like to feed two separate ADS5444-SP ADC's with the same analog signal. The clock to the ADC's would be running at 250 MHz, but 2 nS out of phase, so as to achieve 500 MHz sampling. I'm concerned with sample and hold switching noise from the two channels corrupting the signal.
Can anyone provide any guidance on the best drive electronics to use for such an implementation?
Thanks in advance, Darren O'Connor