This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1101

Other Parts Discussed in Thread: TPS7H1101-SP, TPS7A4501-SP

Hello

I am looking for a space (Radiation Hardness) LDO that will be able to provide at least double the current of my board needs ( Iout > 2x350mA = 700mA)

and to regulate Vin of 5.5-5.6V into 5.2V.

I started with the TPS73601, but it goes only up to 400mA ( < 700mA)  and it will not pass our electronic hardness tests.

Then I looked at the TPS7H1101-SP LDO.

However, at the WEBENCH application on your WEB page, it failed to find a solution at Vin_min=5.5V. Solution was displayed only for Vin_min=5.6V !

I didn't see in the datasheet a hint why the DropOut voltage should be 0.4V for these conditions.

1. Can you suggest an LDO that will provide my needs?

2. Why does the WEBENCH fails to simulate the  TPS7H1101-SP LDO with 0.3V DropOut voltage?

Thanks

Amnon