This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK2711-SP: Power on Sequence when they use it in transmit only mode

Part Number: TLK2711-SP

Hello,

My customer has a question about TLK2711-SP.

[Q]

Please tell me the power on sequence when they use it in transmit only mode.

Is my understanding correct ?

<My understanding>

  1. TLK2711-SP generates a power-on reset under the following conditions.
    • when it exceed the minimum valid voltage (2.375V)
    • valid TXCLK
    • ENABLE is High by the following one of ways
    • It is driven to high by external driver
    • It is high by internal pull-up when It is driven with High-Z by external driver 
  2. LCKREFN is High by the following one of ways
    • It is driven to high by external driver
    • It is high by internal pull-up when It is driven with High-Z by external driver 
  3. LOOPEN is High by the following way
    • It is driven to high by external driver
  4. Wait for at least 1ms until internal power-on reset comple
  5. Changes in Transmit only mode by reset the receiver
  • LCKREFN is driven to Low by external driver

Best Regards,

Hiroshi Katsunaga