This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the LMD18200 block diagram, we see that the current sense circuit is connected to the source of the top MOSFET in both the paths. My customer wants to understand how is the current sensed? Have we used a RDSon based detection or coupled coil method? This is a high side sensing correct?
Hello Mahesh,
Sorry about the delay in response.
The current sensing is neither an RDSon or coupled coil based method.
Please see Section 2.4 on Page 5 in the following app note for more information about the current sensing circuitry of the LMD18200, including a schematic of the current sensing circuitry: AN-694 A DMOS 3A, 55V, H-Bridge: The LMD18200
If this has answered your question, please click the verified answer box so I can close out the question. If not, I will be happy to assist you with any further questions.
Thanks,
Bree Myers