This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for clarification on the current sense and programmable current limit options for the TPS7H1101-SP linear regulator. Between the datasheet and application note, I have come across numerous values for the scaling factor of Ics/Iout. 47394 is in the table, 49917 is in the text and plot of the eval board documentation, then another plot on the datasheet shows three curve providing 48065, 47935, 48150. I understand there is some variability from part to part and operating conditions. The datasheet on pp. 19 discusses PCL and uses a CSR value of 47394 for this calculation. But defines CSR as Ics/Iout. Wouldn't we want Ipcl/Iout, why is CSR defined in this calculation with Ics? Is Ics/Iout and Ipcl/Iout the same? For the high side current sense section on pp. 20. The equation uses the same CSR and a Voffset. But Voffset is in amps, just want to clarify this is really an Ioffset. Also, it appears the Ics offset is 5uA, which would correspond to 0.237 A (5uA * 47394), not 0.1899 A in the datasheet. Could you help clarify the value of Ics/Iout and Ipcl/Iout and the appropriate offsets?
I would like to answers to these questions as well. Also, note that the datasheet minimum value for CSR is a larger number than the one in the "nominal" column.
I would also like to know the correct CSR min, nom, and max values. There is an error in the data sheet as mentioned above. Elsewhere in this forum it is mentioned that CSR nominal is 47500. Are the min and the nom just switched in the data sheet? - Thanks.