This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1101-SP Current Sharing

Hi

My Customer has question.Please Cooperate.

About Figure.21 depicted in the data sheet,

There is a change in the [Total Load] at 4.5A ~ 5.5A.

At this time, the output voltage accuracy is worse?

7242.TPS7H1101.pdf

Regard

T Kishi

  • Hi, Figure 21 indicates the % of the total load (6A) in this case delivered by each of the 2 LDOs in current sharing mode. Between 4.5 and 5.5A, LDO2 is providing a little bit less current than LDO1 but this is not related to output voltage accuracy.

    Thanks,

    JV