This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV8154-EP: Power consumption issue

Part Number: SN74LV8154-EP
Other Parts Discussed in Thread: SN74LV8154

Hi,

I’m having a power consumption issue with a binary counter.

I’m using TI’s SN74LV8154 32 bit binary counter; you may find both the schematic and the actual board attached.

I’m supplying the counter with 2.08V, which should account for the current draw of a few µA (see page 5). Instead I’m drawing 2mA. The counter is fed with a 20MHz pulse; counter outputs nothing (GAL-GBU are pulled to 3.3V). 

Where do 2mA come from? How do I drop it into the µA range? Many thanks in advance, I could really use some help here. I attached a pic of the setup too.

Here are some observations:

It looks like the current draw linearly depends on the input pulse; I don’t remember the exact readings, but I think I had ~0.2mA for 2MHz, ~0.45mA for 4MHz, ~0.6mA for 6MHz. 

If I leave GAL-GBU disconnected, the current draw goes to 2.5mA. Same thing if I’m outputting any of the bytes. It’s not because I’m giving a 3.3V input into GAL-GBU, is it? (I don’t have direct access to the circuit right now to check if it is the problem)