This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825A-SP: UC1825A-SP 1.25V internal voltage

Part Number: UC1825A-SP

I am looking for the tolerance variations  (initial tolerance , temperature, aging, radiation) of the 1.25 V internal which connects to the RAMP pin. Beside the 1.25V could impact the current limit, is there any internal parameters within the PWM IC could cause impact on current limit ?