We are looking to use the TPS3808G33 as a reset supervisor to a Ti DSC. We are looking to implement a 20ms delay and so leaving the Ct pin open circuit.
We require a tight tolerance (+- 10%) of this time over the temperature range -55 to +110. In part 6.6 it states a minimum td time of 12ms and a maximum of 29ms, are these values given over the operating temperature? If so they dont seem to align to the data given in figure 4 which shows a variation of +6% to -1% in the reset time.
Can it be clarified about the tolerance of the timeout time for the IC?
Thanks
Chris