Other Parts Discussed in Thread: , TIDA-00318, BQ500212A
Hello,
I am designing a receiver module using BQ51003 IC and want to test the same with an A11 design A2511 charger pad by Powerport Qi.
I want to test the compatibility between coils, receiver, and transmitter modules for efficiency using the BQ51003EVM-764 board.
As a part of designing, I must calculate the resonant capacitors (C1 and C2) using Ls and Ls'.
My question is, is there any test fixture readily available with PC44 shield and spacers so that I calculate Ls and Ls' for C1 and C2?
Also, even after the calculations of C1 and C2, I wonder how do I use these capacitances in EVM, as these values are fixed to 183nF and 1900pF respectively.
If I am not wrong, I will be getting calculating different C1 and C2 values for different coils.
Thank you in advance,
Best Regards,
Srujana Patel.