This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUC125: Skew data

Part Number: SN74AUC125


My customers request:

I have to handle two 1.8V-SPI-Interfaces (each with 4 signals: CLK,CS,MOSI,MISO) between two components, which are sometimes partially powered. During “power-save-mode”

In order to fulfill the SPI master write timings the skew between the channels is important. The SN74AUC125 is an option. The propagation specification is from 0.5 to 2.1ns. I couldn’t find anything within the datasheet. Therefore following questions:

  1. Is there a specification for the skew between the 4 channels of one SN74AUC125?
  2. Do you have a better suggestion (e.g. another buffer type) to solve the problem?

BR

Frank