Part Number: TXS0104E
Hello E2E,
The datasheet states that when it enter Low into the OE port, each I/O_port will be High-Z.
Each I/O_port has pull-up resistor.
Q1: If the OE has Low, is each I/O_port High?
Q2: Why is Ioz(High-impedance state output current) 2-uA? With a 10-kohm pull-up resistor only, Ioz should be around 100-uA.
Q3: Does the each I/O_port have an internal buffer circuit?
We want to do set to Low for I/O_port when device disable.
Q4: Is pull-down resistor effective on I/O_port?
Regards,
ACGUY