Part Number: SN74LVC8T245
If two different SN74LVC8T245s collide with two outputs, will they break down?
The same signal is connected to the input.
DIR and OE are GND connections.
VCCA = 3.3V and VCCB = 5V are connected.
It's good if the current flows only momentarily,
I hope it doesn't damage the device.
Thank you.