This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC3G07-Q1: Output pin ESD protection structure - Sneak path through the pull-up to the VCC while translating a 3V3 signal to 5V levels

Part Number: SN74LVC3G07-Q1


Dear TI Experts,

in a cost sensitive product there is a 3V3 sensor providing digital signal for a 5V uC, I would like to translate voltage levels with an open drain buffer SN74LVC3G07-Q1:

To calculate the Rp value I would like to ask about the SN74LVC3G07-Q1 output ESD protection structure - here sketched as D1 and D2. 

1. Is there ESD Diode like D1 in the SN74LVC3G07-Q1 buffer

2. Is the D1 behaving like a regular silicon diode with ~0,7V voltage drop or is it a structure which starts conducting at higher voltage?

2. Will there be current flow from 5V through the Rp, D1 to the 3V3 rail? (see yellow highlighted path)